This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: F28377 code to F280045

Part Number: TMS320F28377S
Other Parts Discussed in Thread: C2000WARE

Hello,

Into the previous related post, I asked some solution to reduce cost and size of a project by using a smaller processor than the F28377.

An answer was F28075 or F28045(Sample only now)

Currently, I have a project for F28377 (based on SIDDK to control brushless motor)

Can we directly use all the code (and c2000ware library) without any change to make run the F28377 code into F280075 and 45 controller?

Or we should start a new "hello" projet on new controller and integrate ou code on it?

Exemple: the clock is 200MHz on 28377, 120/100MHz on other...