Part Number: TIDM-1000
Other Parts Discussed in Thread: OPA320, AMC1301, C2000WARE
Tool/software: Code Composer Studio
Assuming that the circuit is stable, vbuspm is 300V. I calculate the vBusPM_ Fdbk according to the parameters on the schematic diagram is 1.7910
The formula is as follows,
According to the resistance R94 R95 R97 R100, we can get VINP = 0.27375, VINN = 0,The amplification is 8.2 times by amc1301 and 0.7978723 times by opa320 to obtain vBusPM_ Fdbk=1.7910
Through ADC sampling, vBusMeas_pu=1.7910 * 0.000244140625 * 717079 / 454 = 0.000691617
But in the data table I gave, when vbuspm = 300, vBusMeas_pu= 0.6776,instead of 0.000691617
Is it me where the calculation is wrong?
Best wish.