This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C28334 PWM Resolution

Expert 3030 points

What is the PWM resolution at 20KHz and 40KHz?  What impact does dead time have on this?

  • Resolution will depend on timer clock frequency as well... .. this is the equation most likely can be used to calculate the resolution

    n = log( timer clock frequency / PWM frequency) / log (2) , where 'n' is PWM resolution in effective number of bits

    For example if you have 20kHz PWM with 50 Mhz clock then PWM resolution is

    n = log( 50 Mhz/ 40kHz ) / log (2) = 10.28 effective bits

    for 20kHz

    n = log(50MHz /20kHz )/ log (2) = 11.28

    Dead band will introduce output distortion but your effective resolution should stay the same.