Tool/software: Code Composer Studio
Hello,
I was able to load the program in flash, but i am observing a strange behavior when i use the flash lnk cmd file.
i am using the example Flash link cmd file which is slightly modified.
BEGIN : origin = 0x080000, length = 0x000002
the application code is updated to be place in flash 4 to7, i have observed it once worked fine even after reset, but later after some time i reloaded after a reset it did not work. on further analysis i observed that at the BEGIN location it was still FFFF FFFF, which should have been some address which will jump to my main function.
Can you please let me know what settings could have been wrong so that i can look around it, or does it mean that FLASH sector is corrupted.
/* Flash sectors */
FLASH0 : origin = 0x080002, length = 0x001FFE /* on-chip Flash */
FLASH1 : origin = 0x082000, length = 0x002000 /* on-chip Flash */
FLASH2 : origin = 0x084000, length = 0x002000 /* on-chip Flash */
FLASH3 : origin = 0x086000, length = 0x002000 /* on-chip Flash */
FLASH4 : origin = 0x088000, length = 0x008000 /* on-chip Flash */
FLASH5 : origin = 0x090000, length = 0x008000 /* on-chip Flash */
FLASH6 : origin = 0x098000, length = 0x008000 /* on-chip Flash */
FLASH7 : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */
FLASH8 : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
FLASH9 : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
FLASH10 : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
FLASH11 : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
FLASH12 : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
FLASH13 : origin = 0x0BE000, length = 0x001FF0 /* on-chip Flash */
// FLASH13_RSVD : origin = 0x0BFFF0, length = 0x000010 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */