Part Number: TMS320F28377D
Other Parts Discussed in Thread: CONTROLSUITE, LMR10510
Hi,
I am having issue with loading firmware into flash with my own board, loading into RAM is ok. Below is the error message. The voltage regulator's current ratings for 3.3V and 1.2V are sufficient. Please help me out what would be the reason casing these issues? Thanks in advance.
C28xx_CPU1: GEL Output:
Memory Map Initialization Complete
C28xx_CPU1: If erase/program (E/P) operation is being done on one core, the other core should not execute from shared-RAM (SR) as they are used for the E/P code. Also, CPU1 will be halted to determine SR ownership for the CPU which will run the Flash Plugin code, after which CPU1 will be set to run its application. User code execution from SR could commence after both flash banks are programmed.
C28xx_CPU1: Error occurred during flash operation: Timed out waiting for target to halt while executing wr_pll.alg
C28xx_CPU1: Error writing the PLL values (Flash algorithm timed out). Operation cancelled.
C28xx_CPU1: Perform a debugger reset and execute the Boot-ROM code (click on the RESUME button in CCS debug window) before erasing/loading the Flash. If that does not help to perform a successful Flash erase/load, check the Reset cause (RESC) register, NMI shadow flag (NMISHDFLG) register and the Boot-ROM status register for further debug.
C28xx_CPU1: Trouble Removing Breakpoint with the Action "Remain Halted" at 0xc0eb: (Error -1066 @ 0xC0EB) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 9.1.0.00001)
C28xx_CPU1: File Loader: Memory write failed: Unknown error
C28xx_CPU1: GEL: File: C:\ti\controlSUITE\device_support\F2837xD\v210\F2837xD_examples_Cpu1\blinky\cpu01\ccs\CPU1_FLASH\blinky_cpu01.out: Load failed.
Cindy