Tool/software: TI C/C++ Compiler
Hi all,
I am trying ti design the C2000 experimenter kit/ Docking station using the Revised 3 schematic. In the schematic there are two boot pins. For 2833xx boot 3*4 pin headers in the schematic there are GPIO-84;GPIO-85;GPIO-86;GPIO-87 label. But I didn't find those labels where they are connected in DIMM-100 or any other component (Please see the scematic attached.). Do I need to worry about?
Your help is appreciated
Sincerely
Ashik AminUSBDockingStation_Schematic_[R3].pdf