Hello Champs ,
please I have a digital control app where I must as much efficient as I can .
28033 including CLA for the control is running full speed @ 60 MHz .
one idea can be to put all the control code in RAM and put Flash in stdby to save current .
I saw stby to active for flash is automated if you access flash location and you have a wakeup time fixed by
FACTIVEWAIT register . please which is the minimum value I can put here , I am not able to find this data in the datasheet ... what about the minimun delay I can expect from flash in sleep ? thank you very much bye Carlo