Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: TMS320F28379D, CC1310, C2000WARE
Hi there,
I am working on a solution where I need to send data over SPI from CC1310 to TMS320F28379D (I'm going to call this guy 283).
Where CC1310 is the Master and 283 is the Slave, there are no other components on the SPI network.
I am having trouble receiving data on 283 as he does not read any data on the receiving buffer.
I need to transfer 10 different numbers, each between 0 and 4096, one way.
I have tried using the spimaster example for CC1310 and the spi_loopback_cpu01 example for 283, adjusting the pinouts, changing receiving and sending datatypes but I do not see anything turning up on the 283's Receiving buffer.
Can anyone help with a bit of code by any chance?
Regards,