Tool/software: Code Composer Studio
Hi,
I am using TMDSCNCD28379D control card and only using it for generating PWMs signals in an open loop. It was working fine but something happens and receives no PWM from the pins. I have connected the controlboard and control card with my laptop to download the control program again to generate the same PWM but I started to face error, which is '
IcePick_C_0: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If the error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.576.0)''.
I have also tried to lower the TCLK but nothing works. additionally, the control card is getting hotter than normal. Please help to solve the issue. Thank you