Hi All,
I am hence contacting you for some more information on the TIDM-1000 board.
In particular, the question is whether you think it can work with a network frequency of 360-800Hz.
I looked at the documentation and found no limit in this regard even if you specify all the tests were done at 60Hz.
I have seen, however, that the FW platform allows the switching frequency to rise above 100KHz which we consider indispensable to manage a higher network frequency.
Who can please give me answers on this?
Obviously changing the frequency customer will surely have to change a bit of circuitry starting from the inductors but I am interested in knowing if the conditioning circuit (sensors and dsp) can manage higher frequencies.
In the past the E2E post for this topic for the same customer was the below: https://e2e.ti.com/support/power-management/f/196/p/851645/3151632#3151632
Many Thanks,
Antonio