This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/C2000WARE-DIGITALPOWER-SDK: Boost/Sepic example

Part Number: C2000WARE-DIGITALPOWER-SDK


Tool/software: Code Composer Studio

Hi,

I wondering if there will be a example project like the DC-DC Synchronous Buck Converter for a boost or sepic device in the Digital-Power-SDK.

If not, do you think it is possible to modify the buck example to use it as a boost?

Where are necessary lines in the software code to modify?

Thanks and best regards

David

  • David,

    I am not aware of any plans to add such an example.

    The buck example is a reasonable starting point for developing a boost solution.  I think the primary difference would be the inverted nature of when energy is being transferred to the output stage relative to the PWM signal.  Depending on the hardware, the software changes might be limited to a few timing adjustments for noise mitigation.  The control loop would need to be adjusted as well, of course.

    -Tommy