Part Number: TMS320F28377D
Hello,
I am using the 12 bit ADCs at a sampling time of 15kHz to monitor voltages through a resistor divider. It seems that the ADC sampling is pulling the input signal lower. Using same method for other ADC inputs do not show this issue. I have a 10V source divider through a 33.2k and 10k resistors and a 0.1uf filter cap. The input to the ADC is expecting 2.3V but for some reason its being pulled down to about 2V. Is there something inside the ADC that I am missing or that could be causing this?