This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: Power up sequence

Part Number: TMS320F28377D

Hello experts,

I got question about power-up sequence from customer.

From datasheet, there are some requirement in below;
1.) The 3.3-V supplies should be powered up together and kept within 0.3 V of each other during functional operation.
2.) During the ramp, VDD should be kept no more than 0.3 V above VDDIO.
3.) The supplies should ramp to full rail within 10 ms and supply ramp rate should be larger than 330V/s.

The sequence limitation between VDD(1.2V) ramp and VDDIO(3.3V) ramp is only 2.). Is it correct?
For example, is it no problem to take some time (100ms ~ few seconds) between 3.3V ramp and 1.2V ramp?

I would appreciate if you would give me advice.

Thanks and best regards,
Ryo Akashi