Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
We can't find the resouce parameter of CLB and CLA,how much is it?Such as how much byte for CLB,how much RAM for CLA?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
We can't find the resouce parameter of CLB and CLA,how much is it?Such as how much byte for CLB,how much RAM for CLA?
Pls refer to datasheet "TMS320F2838x Microcontrollers With Connectivity Manager datasheet (Rev. B)"
Section-3 Device Comparison for CLB details.
Section-6.3.1 C28x Memory Map for CLA memory details
Hi,
CLB tile has different logic blocks like LUT, counters and state machine etc. Detail information about this is provided in section "9.4 CLB Tile" of device TRM. And there are 8 instances of such tiles on this device.
Regards,
Vivek Singh
I have checked it. "There are three LUT4 submodules in each CLB tile".
it means it just support 8*3=24 LUT?if so ,the resource is too limitied,how can it support BISS-C and Endata at the same time?
“Note that the CLB module can onlybe accessed via library functions provided in the PM EnDat22 Library and not otherwise configurable by
users.”
i am evaluating whether i can use CLB to support Endate,biss-c,and most postion encoder protocols.
some questions need your help:
1,whether user ourself can use CLB to develop fucntion to support Endate,biss-c and other protoco?Or user must use TI Position Manager Library such as EnDat22 ?
2,how much resoure does Endate need for CLB and MCU?how can i evaluate whether resouece is enough?
3,if i have to use TI Position Manager Library, is it free?
We'll have our CLB expert look into these queries and provide you the response.
Regards,
Vivek Singh
Hi,
longfei zhang said:1,whether user ourself can use CLB to develop fucntion to support Endate,biss-c and other protoco?Or user must use TI Position Manager Library such as EnDat22 ?
longfei zhang said:2,how much resoure does Endate need for CLB and MCU?how can i evaluate whether resouece is enough?
longfei zhang said:3,if i have to use TI Position Manager Library, is it free?
2,how much resoure does Endate need for CLB and MCU?how can i evaluate whether resouece is enough?
TI library consumes 3 tiles for EnDat and 2 tiles for BiSS-C and 1 for T-format.
As i konw,F28388D just have 8 tiles for CLB,it will be very limited to support all protocols such as EnDat、BiSS-C、T-format、Nikon、Tamagawa、Sanya and so on.Can i duplicate tiles as my customers will not use these protocols at the same time?
Hi,
longfei zhang said:Can i duplicate tiles as my customers will not use these protocols at the same time?