Part Number: TMS320F280049
Hi expert
According to TRM of 28004x, GPIO22/23 are analog mode at reset.(in section 8.1 Note)
However, in the description of GPAASEL, GPIO22/23 are digital mode at reset.
is there any conflict of this?
We are using the internal 1.2V Switching Regulator DCDC of MCU now,
we want to know if it is necessary to configure GPIO22/23 as anolog mode when using it?
And if yes, should we have to configure GPIO22/23 as anolog mode in GPAASEL?
Or it is the default analog mode, and there is no need to configure?
BTW, we notice that in the next generation product, this VREG is removed, what is the concern?
Thanks for your help.
Linna