Part Number: TMS320F28379D
Other Parts Discussed in Thread: TIDM-1010
Hi,
About "TIDM-1010 : BiSS-C Absolute Encoder Master Interface Reference Design for C2000 MCUs reference design", TMS320F28379D is used.
My customer would like to know if the FW can be migrated to fewer pin count and smaller package size C2000 IC( < 10mm*10mm).
If the answer is "Yes", please help to provide the suggested C2000 IC P/N which also can access two BiSS-C Absolute Encoder Master Interface
Thanks.