Part Number: TMS320F28377D-EP
Other Parts Discussed in Thread: OPA333, TMS320F28377D
Hi ,
I am using OP-AMP based sensing circuit. The OP-AMP is powered using VCC=3 V.
The internal ADC is used for conversion purpose which uses external reference voltage VREF_3V.
My doubt is if the OP-AMP circuit power ups first and gives input to ADC before ADC receives the reference voltage (VREF_3V). Does it cause any damage to ADC input stage.
I am using different power supply for OP-AMP and ADC reference so it may not be synchronized.
Reference block diagram:
Thanks,
Namita