Hi Guys again LOL. SERIOUS PROBLEM.
I'm connecting a 4MB (Megabyte) SRAM on the EMIF F28377D and while assigning the address lines I find that address lines 20 and 21 are missing from the manual.
The manual says that there are 22 address lines which means to me EM1A0 to EM1A21 which equals 22 address lines equal to 4MB's of address space but the manual only lists EM1A0 to EM1A19 address lines. I even did a search in the PDF for EM1A20 and EM1A21 and search said NOT FOUND. Where is EM1A20 AND EM1A21?
Please let me know. This will be a project breaker if I can't get 22 address pins like the manual says. Well I guess I can get away with 2 meg which is 21 address lines but 20 address lines is only 1MB, not enough.
I know I can use PORTA as the address lines and PORTB as the data lines but the IO PORTS top speed is only 25Mhz, the EMIF is 100Mhz.
Pete :)