Part Number: TMS320F280049C
Other Parts Discussed in Thread: UNIFLASH
Using Uniflash 6.0.0.2710 and F280049C. With a given Hex file, the F280049 can be programmed and operates correctly. However, when you export in Uniflash, it will swap the bytes in the exported file. In CCS, you can export the memory and it provides an option to swap. This does not appear to be available in Uniflash, so believe there is an issue here. Desire is to program the F280049, export, and reprogram from exported file without the need to byte swap via a hex utility. Please let me know if more details are needed.
Thanks,
Eric