This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: Fast data transfer from DMA to CLA

Part Number: TMS320F28377D

Hi team,

Here is one question about fast data transfer between DMA and CLA.

My customer is using DMA to get the result of ADC(@400kHz), but their control loop runs in CLA(@100Khz). And the the control loop needs the ADC sampling result.

Our question is:

1. Can DMA directly access to CLA Data RAM? If it is possible, then we could leverage DMA to transfer ADC result directly to CLA data ram, then no additional operation would be needed for CLA to use ADC result.

2. If the answer is no, what is the recommended way to implement DMA and CLA for such a scenario?

Regards,

Brian

  • Brian,

    Regarding your question 1, it is not possible on TMS320F28377D device.

    You can directly access the ADC results from CLA. That would be the simplest way to implement the control loop using CLA & ADC

    Regards,
    Praveen

    Note: If my post answers your query, please click "This resolved my issue" button.

  • Brian,

    CLA has access to highlighted RAM memory shown below. Which memory are you talking about when you say CLA data RAM? We have CLA data ROM not CLA data RAM.

    We don't have any memory location which has both CLA / DMA access at the same time. Please check Pg 182. Table6-1. C28xMemoryMap for more details www.ti.com/.../tms320f28379d.pdf

    As Praveen suggested, CLA can access ADC result register directly.

    Regards,

    Manoj

  • Hi team,

    Thanks for the quick reply. 

    Yes we are aware of the idea that CLA could be used to access CLA. But the problem is ADC ISR and control ISR would overlap. 

    Another idea is that ADC ISR runs in CPU1 CLA and control ISR runs in CPU2 CLA. But according to our understanding, these 2 CLA also cannot share access to a common RAM. In this way, the data flow would be CLA1(ADC Sampling)->CPU1->CPU2->CLA2(control SIR). And this is obviously not what we hope to achieve.

    Regards,

    Brian

  • Brian,

    You can also keep the ADC ISR running from CPU and consume the ADC result data inside the CPU1 CLA task.

    Regards,
    Praveen

    Note: If my post answers your query, please click "This resolved my issue" button.