Part Number: TMS320F28335
Hi
I am working on serial flashing on 28835 custom board.
I am using SD flash software for serial flashing.
All the settings related to SD flash has been set as per " TMS320F28xx SDFlash Serial RS232 Flash Programming Reference Guide".
boot mode selection in my custom board is set as per SCI boot mode selection pins.
the problem is, when i press reset button in SD flash tool, i am getting following message
MSG: Interface version 1
MSG: Unloading driver
MSG: Reloading driver
MSG: User must now get target to bootload state
MSG: Interface version 1
After this, even we tried to reset the dsp manually. even after it is showing same message.
if we try to flash, it says following message
ERR: Failed connection to the target
So guys, what might be the problem.
how can i reset the device.