Part Number: TMS320F28388D
Tool/software: Code Composer Studio
Hi All
The program is running without connecting to the emulator. How to connect the emulator to see where the program is running?
Best regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28388D
Tool/software: Code Composer Studio
Hi All
The program is running without connecting to the emulator. How to connect the emulator to see where the program is running?
Best regards
Hi,
You can launch the target configuration file and then connect to the core and check the PC value.
Make sure you remove the Gel file from target configuration file so that core does not get reset during CCS connection. You can double click on target configuration file and then click on the core which you want to check and remove the Gel file and save the updated configuration file and then launch it.
Regards,
Vivek Singh
Hi,Vivek Singh
Do not know how to operate, can you give the specific operation?
或者写成图片的形式
Or in the form of pictures
Best Regards,
Hi expert
This method can solve the connection problem of CPU1 core. Cm core still resets in this way
Best Regards,
You need to delete the Gel file for CM core as well. Each core has it's own Gel file.
Regards,
Vivek Singh