hi expert,
I want to use FSI at SPI mode, but from TRM. there is some restriction on SPI mode.
for example, it can only support 16 bit length. and only support one mode:
Data will transmit on rising edge and receive on falling edge of the clock.
So does this means, when FSI uses as SPI, the other side should do some special process,it must be another MCU or processor? is this possible to connect to an ADC such as ADS129X.
BR
Emma