This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069: Enabling interrupt from different group (e.g, "timer 0 INTERRUPT(from group 1)" and "PWM INTERRUPT(from group 2)".

Part Number: TMS320F28069

Hi,

I am trying to generate two interrupt from "timer 0 " and "pwm".

So, writing below line will enable both the interrupt or there is another procedure.

IER |=M_INT1;

IER |=M_INT2;

OR

IER |=0X0011;

which line will enable interrupt from both group's?

Thank you

  • Hi Mihir,

    mihir dave said:
    which line will enable interrupt from both group's?

    The first method you have described above will set the correct value of the Interrupt Enable Register (IER)

    IER |= M_INT1;    // Group 1

    IER |= M_INT2;    // Group 2

    You could also do something like this to enable both:

    IER |= M_INT1 | M_INT2;   // Group 1 & 2

    The second method you described could be altered in the following way:

    From: IER |= 0x0011; // INT1 and INT 5

    To: IER |= 0x0003;  // INT1 and INT2

    The IER is a 16 bit register as follows:

    Don't forget to modify your PIE Control Register afterwards. Also ensure to enable the Global Interrupt INTM (EINT) and global real time interrupt DBGM (ERTM). 

    Best Regards,

    Marlyn

     

  • Hi Marlyn ,

    Thank you very much doubts are cleared now.