Part Number: TMS320F28388D
Other Parts Discussed in Thread: TMDSHSECDOCK, TMDSCNCD28379D, TMDSCNCD28388D
I am attempting to use the EMIF1 interface on the TMS320F28388D paired with the TMDSHSECDOCK to interface with an external parallel nor flash chip.
I am accessing the EMIF interface signals via the header pins on the TMDSHSECDOCK docking station, but it seems that not all address and data pins are accessible. Particularly EMIF1_A7 and EMIF1_D9.
EMIF1_A7 uses GPIO47 or GPIO51. GPIO47 is not available on the TMDSHSECDOCK, and GPIO51 is used by EMIF1_A11 which has no other mux options. This leaves me not able to use both A7 and A11 address lines in the interface.
EMIF1_D9 (GPIO75) is simply not present on the TMDSHSECDOCK so I have no way to connect this data line to the flash memory component.
Is this an oversight that a couple of signals are missing on the interface or do I not have the correct diagram for the headers?