This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320F28388D: What is the substitute of the compiler source file frexp.c for compiler V20.2.1.LTS?

Part Number: TMS320F28388D


Tool/software: TI C/C++ Compiler

Hi TI,

I need to use frexp.c for creating a run-time library but couldn't find the source file of the same name in the current compiler version, V20.2.1.LTS.

Is there any substitute file is present?

What is the name of the file?

This file contains the frexp() library function which breaks a floating-point number into a normalized fraction and the integer power of 2.

Could you please tell.

Thanks in advance

Gurusha