Part Number: TIEVM-VIENNARECT
Other Parts Discussed in Thread: TMS320F28379D, SFRA, TIDM-1000
Tool/software: Code Composer Studio
We are trying to evaluate the TIDM_1000 for use in development of our own 3 phase PFC power supply using a c2000 MCU.
This is the first time using a TI MCU or CCS.
So far we have had many issues with getting the project to run in ccs v10.1, xds100v2 probe, using a TMS320F28379D, project was installed with C200ware_digitalpower_SDK-3.00.01 and our input source is a 3 phase 0-480VAC variac.
When we are able to get the debugger and the project builds to run, we are not getting consistent output results, we have tried all 4 builds, with and without CLA with very limited success.
We have not edited any of the project files and only changed values in the GUI for the project; build level, power (corresponding to external load changes) and ran the SFRA when the project was running, though we had freezing and crashing with SFRA also.
Connection tests of the MCU communication and debug probe pass, however 4 out of 5 times approximately we are getting 1142 errors when trying to run and/or crashes of ccs.
We have tried this on 2 different windows PC, also multiple project work spaces starting over with the process.
The only build that successfully had a PFC close to 0.99 at 208VAC input was build 3, though it took multiple tries to get it to run successfully.
All other builds, when successfully ran on the system failed to power factor correct at the 208VAC input voltage, some would have distorted line currents when boosting the output load voltage and often not reach 600VDC out or output voltage would appear unstable unless we reduced our input voltage to around 50%.
We are attempting to follow the TIDM design guide instructions exactly, though have found some gaps in the documentation and through research and trial and error solved some issues.
I am questioning if our TIDM_1000 has some hardware issues or the download(s) are corrupted perhaps even the project is not compatible somehow with our software versions.
Any assistance or pointers in the right direction would be appreciated.