Part Number: TMDSCNCD28388D
Other Parts Discussed in Thread: C2000WARE
Dear sir and madam,
I am using TMDSCNCD28388D F28388D controlCARD. I have a problem of connecting controller.
The popup shows that my controller did connect to TwinCAT 3 because 'Ethernet - TwinCAT-Intel PCI Ethernet Adapter (Gigabit)' is in 'Installed and ready to use devices(realtime capable)'. However, when I scaned, there was no 'Device 1 (EtherCAT)' to sellect, it only had 'Device 1 (EtherCAT Automation Protocol)', that is why the icon is blue not red. Moreover, you can see that Adapter in 'Device 1 (EtherCAT Automation Protocoll)' connected correctly to the controller because the IP adress was 169.254.212.254, but there was no 'Box'. I did try to right click on 'Device 1 (EtherCAT Automation Protocol)' and then scaned but there was also no 'Box'.
The main problem is no 'Box'. How could I make it have 'Box' in Device?
Best regards.