This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320F28379D: Garbage value in structure array

Part Number: TMS320F28379D

Tool/software: TI C/C++ Compiler

Hi,

I have a global structure declared as 

struct Data{
int userdata[5];
char name; 

};

I have created an object for the structure as : struct Data Mytime LAinfo ;  

 When the program runs initially when i print the values of Mytime.userdata[0] , it prints a garbage value of 15528 . This garbage value occurs every time until later on when I initialize the array elements. 

This  does not seem to be the problem with the other structure objects such as LAinfo.userdata[0] . 

Kindly let me know what is causing this garbage value to be stored in only one of the structure variables and not all. 

Also, as per general information I believed that global variables are initialized to 0 be default. 

 

Thank you