Customer is planning to use TMS320F28335 in an aircraft-related program. They need to be able to configure the CAN peripheral to conform with ARINC 825. The ARINC 825 specifies the following requirements:
1) The SJW (Synchronization Jump Width) SHALL be one time quanta.
2) The sample point SHALL not be less than 75% of the bit time width.
3) Only one sample point SHALL be used.
How do you setup the CAN Bit Timing Configuration register to satisfy these requirements?