This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C ADC issue



Hello all:

I am using DSP-TMS320F280049C for software development. When Debugging ADC module, I encountered a problem:

  • The 10th  pin of the DSP chip ( the function is ADC-A3), when no signal input, a 3.62V level is detected above the pin.

    • This level still exists after I try to erase the flash program. And I still measured a 3.62V voltage signal on the pin after I dropped it.

Is there any other function of this pin or is the level of this pin related to the chip peripheral configuration circuit?

Thank you!

Due.Yuan