Part Number: TIDM-1007
1.What's the use of __TMS320C28XX_CLA__?
2.When using CLA, need I add this into pre-define name?
3.When I add this to pre-define name and choose CONTROL_RUNNING_ON == CLA_CORE, the compiler suggest a large amount of error. Why?
IF I do not pre-define __TMS320C28XX_CLA__, the code do not use CLA-related libraries and include files, such as "DCLCLA.h".