This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280041C: not recognizing flash bank 1 in ccs flash settings

Part Number: TMS320F280041C

Hi,

I am using TMS320F280041C and as per data sheet we have two banks. I want both the banks to be used but in the flash settings i am able to see only bank 0 but not bank 1

below is the screenshot:

Hence when i am trying to flash for Bank 1 address i.e (0x090000 - 0x9FFFF) it is throwing error as data verification failed since i don't have access to flash bank 1.

I checked the gel file f280041c.gel where there is only flash bank 0 defined. i tried to modify gel file by adding details for flash bank 1 but dint get any luck. request to please look into this issue?

Thanks and Regards,

Suhail.B