This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSCNCD28335: Using DRV8312evm with f28335 control card ?

Part Number: TMDSCNCD28335
Other Parts Discussed in Thread: CONTROLSUITE, DRV8312

Hi,

is DRV8312evm compatible with f28335 control card. I have used the above inverter module with 28069 control card. However, on exploring f28335 control card, I found the pin details to be different form that of of 28069control card. I wanted to know whether I can use f28335 control card with DRV8312-evm. If yes, what pin configurations need to changed.

  • Yes, it is. That depends on what example code and peripheral pins are you using. You might find the schematic and pin map table of both kits in controlSUITE to change the configuration code in the example project.

    ControlSUITE

    https://www.ti.com/tool/controlsuite

    DRV8312:

    \ti\controlSUITE\development_kits\DRV8312-C2-KIT_v128\~DRV8312EVM-HWdevPkg

    F28335controlCARD:

    C:\ti\controlSUITE\development_kits\~controlCARDs\CC2833xHWdevPkg