Part Number: TMS320F28027F
Hi,
My question is related to JTAG circuitry on PCB. First I copied the schematic mentioned on page 25 of tmsf2802x datasheet. According to suggestion, additionaly I had to add DIP switch for TRST, TDO and GPIO34 with pull up and pull down resistors as shown in picture below
1) Normally for the normal operation of MCU, the TRST' should be at high or low state?
2) The TRST' will be connected to 3,3 volts when switch is on. Is that safe to use?
3) As it can be seen from Launchpad f28027f, there are Tx and Rx pins for communication but in the devices manuals, I have not seen these pins for communication with JTAG. Which type of communication will be done with xds110?
4) The GPIO34, TDO and nTRST are connected to JTAG header and their respective pins of MCU with pull down resistor of 2.2k. Is that fine diagram for JTAG?
Thank You