This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/DRV8312-C2-KIT: Example Program: BLDC Sensorless not running

Part Number: DRV8312-C2-KIT

Tool/software: Code Composer Studio

I have went through the HowToRunGuidev101.pdf provided with control suite for the motor kit. I am working on CCS 10.1, and all the switches and jumpers have been set, at the same place that the guide has told me to set them. 

I have setup the target configuration like this:

I was able to enter the debug mode successfully, and insert all expressions and charts into the code composer studio. I also turned on real time silicon mode, but when running the project it would not run.