This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS2MTRPFCKIT with F28035 ControlCARD Demo Code using the CLA?

Other Parts Discussed in Thread: CONTROLSUITE

Does the demo code that comes shipped in the TMDS2MTRPFCKIT with F28035 ControlCARD Demo Code utilize the CLA, or is it just fixed point?

  • The code in controlSUITE just uses the 28x CPU. However, the HVMTRPFCKIT shows the code for doing the PFC in the CLA.  We also have an example of the CLA on the 2MTRPFCKIT running one of the motors, but we haven't released.  We will eventually clean it up and put it into the official controlSUITE structure (we are also planning a HW revision of the kit with a new DRV83x2 driver chip and CAN/SPI connectors).