Part Number: TMS320F28379S
according to the Tamagawa T-Format Absolute-Encoder Master Interface Reference Design
for C2000™ MCUs, I can setup gpios as needed depending on which spi clock I choose to use. Fine.
But in a couple places, the reader is told that GPIO7, and GPIO34 must always be configured.
I want to use the f28379s with the 100-pin package. I do not have neither gpio7 or gpio34. Please clarify the meaning here- if I want to use the t-format example software I must use a version of f28379 that includes those two pins? I am not able to work around this?
Thank you,
Don Morgan