Part Number: TMS320F280045
Hello,
is it possible to create one direction communication using FSI?
My idea is to have sensor (FSI master) which has FSITX and FSICLK signals and sends data to another FSI Device (slave) which has FSIRX and FSICLK input pins.
In TMS320F28004x reference manual I found only the SPI compability mode which doesn't suit my application (I cannot waste mcu time by encoding FSI frame to SPI frame) and note 28.5.1.2 Establishing the Communication link from which I understand that when I want to establish communication between two FSI modules I need both RX and TX signals on both master and slave devices.
Thank you,
Jan