Part Number: TMS320F28069M
Dear experts,
Maximum ADC Clock is 90M or 45M?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yamazaky,
You are correct that the effect of 0,0 in these bits will be that ADC Clock = System Clock. If System clock is >45Mhz then this is unsupported configuration. You will need to write to the CLKDIV2EN bit in this case to make the ADC clock 45MHz when System clock = 90MHz.
Best,
Matthew