Part Number: TMS320F28388D
Tool/software: Code Composer Studio
Hi TI.
I have got a task where i need to take an old code that works on TMS320F28M36 and put it over on the new board TMS320F28388D.
I am having a lot of trouble regarding the libs and GPIO's.
I cant seem to find any GPTM on the new board that matches the old one.There are also a lot of the .h files i cant find. Such as hw_ethernet.h.
It is a large program that talks with labview, controls some IGBT modules and read some measurements.
Do you have a good proposal for me? Where to start?
It is like on the Old board the CM-core was the master core but now it has changed to the c28-cpu1?
Is it also true that you made new configurations for the GPIO?
BR
Asbjørn Schram Anneberg