Part Number: TIDM-1022
For 2-phase Interleaved operation, does below configuration generates interleaved PWM on PWM1A(Phase1) and PWM1B(Phase2) ?
I can understand the interleaved PWM generation with symmetric(up-down) mode.
But, ePWM1 is configured for Up counting mode in this. I did not get that.
Can you please explain how it is generated?
// Set actions
//do nothing to T1 and T2 at the beginning
EPWM_setAdditionalActionQualifierActionComplete(base1, EPWM_AQ_OUTPUT_A,
EPWM_AQ_OUTPUT_NO_CHANGE_DOWN_T2);
EPWM_setActionQualifierActionComplete(base1, EPWM_AQ_OUTPUT_A,
EPWM_AQ_OUTPUT_NO_CHANGE_UP_CMPB);
#pragma diag_suppress 190 // suppress warning 190
EPWM_setActionQualifierActionComplete(base1, EPWM_AQ_OUTPUT_A,
EPWM_AQ_OUTPUT_LOW_UP_CMPB | EPWM_AQ_OUTPUT_HIGH_ZERO);
#pragma diag_suppress 190 // suppress warning 190
EPWM_setActionQualifierActionComplete(base1, EPWM_AQ_OUTPUT_B,
EPWM_AQ_OUTPUT_LOW_ZERO | EPWM_AQ_OUTPUT_HIGH_UP_CMPA);
/* Loading of the compare registers from duty cycle*/
ePwm1Cmpa = ePwm1Cmpc - ePwm1Cmpc*dutyPU;
EPWM_setCounterCompareValue(EPWM1_BASE, EPWM_COUNTER_COMPARE_A, ePwm1Cmpa);
// update channel B
ePwm1Cmpb = ePwm1Cmpc*dutyPU;
EPWM_setCounterCompareValue(EPWM1_BASE, EPWM_COUNTER_COMPARE_B, ePwm1Cmpb);
Thanks,
Piyush