Part Number: TMS320F28388D
Other Parts Discussed in Thread: TMDSCNCD28388D, C2000WARE
This query deals with debugging options for the 28388D chip.
It is understood that 28388D's C28 cores are compatible with each of the three families of debuggers: XDS100v2, XDS200 and 560v2. (All three are provided by Spectrum Digital and Blackhawk)
CM, which is an ARM-Cortex M4 core, has 2 separate debug ports: SWO and 5 pins Trace port.
1. Regarding the C28 cores: What would be the advantages, if any, of using each debugger family with 28388D? Specifically, would there be more tracing capabilities with the more advanced families?
2. Regarding CM: What are the pros/cons of working with any of the two debug ports? Does the trace port provide more tracing capabilities relative to SWO?
3. Which of the three families of debuggers above, if any, can work with both core types? and with which of the two debug ports in CM?
If none, does it mean that two debuggers are required: One for C28's cores and one for CM?