This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F280025: Sysconfig Pinmux None Option?

Part Number: TMS320F280025
Other Parts Discussed in Thread: SYSCONFIG

Tool/software: Code Composer Studio

Software Team,

Ok, this sysconfig thing is really cool.  Kudos to the team for supporting this and also to the CCS guys for the implementation.

In playing with it, one shortcoming I'm seeing is it lacks an option for not assigning a peripheral function to a pin.  For instance, I've got some serial peripherals pinned out and one of them is using GPIO1.  I'd also like to use EPWM1 but only bring out the A to GPIO0 and not use the B channel at all.  There should be an option in the pinmux drop down that allows this and it isn't there.  Instead it tells me I have pin conflicts because it won't let me not use the B channel.

I'm 99% sure you're already aware of this short coming, but on the 1% chance you're not I thought I should bring it up.

Best,

Trey