Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
When I use CCS V10 software and tms320f28377d is used as the chip, two projects are set up for two CPUs in CCS. Each time I click debug to burn code into DSP, a code file will be directly burned to two CPUs. Open the project file of two CPUs at the same time. When the mouse stays in the project file for the last time, the code of the last mouse stay will be burned to the two CPUs.
How can I do this, open the engineering files of two CPUs at the same time, and burn the code of one CPU to the specified CPU at a time.