This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28375D: TMS320F28375D hold CPU2 in reset

Part Number: TMS320F28375D


Hello,

I am working on the TMS320F28375D. I have done some searching on the forums here and have looked in the data sheet but couldn't find a clear answer.

I am trying to figure out how to hold the second core on this processor in reset. I currently have a system configured with a core 1 and core 2 and both are running but for specific reason I need to be able to dynamically hold the core 2 in reset.

I did find some information on the data sheet which lead me believe I probably need to use the IpcRegs.IPCBOOTMODE but I'm not sure because it doesn't have any information on the bits of this register. It just says 'This register is used by CPU1 to pass a boot mode information to CPU2".

If anyone can point me to where to look, that would be highly appreciated.

Thank you