This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-F280049C: LAUNCHXL-F280049C & Programming F280048

Part Number: LAUNCHXL-F280049C


Tool/software: Code Composer Studio

Hi, my name is Iulian Popa.

I´m a student from Univerity of Zaragoza in Spain. Im using one of your development board 'LAUNCHXL-F280049C' and I have some questions and problems. First of all I´m using the follow:

-  CodeComposer version 9.3

-  C2000Ware version 3.1.0.00

As I was saying, I´m having problems when I´m trying to write into my program into F280048 FLASH memory. I have my project developed using driverlib stuff into LAUNCHXL-F280049C but all GPIOs and signals are programmed to fit for the F280048 (F280048 is in solded in an external PCB). To program into RAM memory of the F280048 the code i´ve developed I´m using the XDS100 debug probe from the LAUNCHXL-F280049C using the 2 pin advanced mode (TMS, TCK and GND) to program the F280048. 

My question is: How can I program the code developed in the FLASH of the F280048 microcontroller using the XDS100 of the LAUNCHXL? What steps should I do to be able to write my code in the FLASH memory of the F280048 through the XDS100 of the LAUNCHXL-F280049C?

I hope my question is understandable :D.

Regards, Iulian.