This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: No response to IPC interrupt using BIOS system

Part Number: TMS320F28377D
Other Parts Discussed in Thread: SYSBIOS, C2000WARE

My customer is developing F28377D, now they meet issues on IPC usage using BIOS system.

The basic operating system is below:

CCS Ver.:9.3.0

Compiler Version:TI v18.12.4.LTS

BIOS Ver.:6.76.03.01

There is a large amount of data exchange between CPU1 and CPU2, which is currently controlled by the timer + IPCFlag method. I want to use timer + IPC interrupt to control. Refer to the dual-core IPC interrupt routine given by TI, adding IPC interrupt in the SYSBIOS version, but there is no response.

TI reference code is:

C:\ti\c2000\C2000Ware_3_02_00_00\device_support\f2837xd\examples\dual

cpu01_to_cpu02_ipcdrivers and cpu02_to_cpu01_ipcdrivers

Customer code can provide in email if needed.

BTW, Could you kindly give customer some check lists to debug?

BR

Emma