Part Number: TMS320F28377S
Hi.
I port ucos-II programs in TMS320F28377S,find that if I switch tasks in the interrupt ISR (e.g., perform OSQPost() in timer0 ISR to get task A ready and switch to task A), the next time Timer0 ISR will not respond until task A has been executed.
I think the reason which prevented the entry of the next interrupt is that time0 ISR did not complete when switching task A-------The instruction "asm(" TRAP #16")" in OSIntCtxSw() will be executed directly even if the global interrupt is masked(INTM = 1).
How can I solve this problem?