This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-02008: Dimension of the reference design board

Part Number: TIDM-02008

Hello,

Can you please tell me the dimension of this (TIDM-02008) reference design (i.e. Length, Width and Height in mm)? I could not find it in the user manual. 

Thanks. 

  • You can refer to the hardware files in altium for the size of the board. Below is the density we got, but there is definitely more density possible with a more optimized layout. The heigh assumed is the max height of the cap which is 40mm, the control card height is higher but it can be easily re-designed to meet this requirement. 

    3300/(244mmx 85mm x 40 mm) = 65W/inches^3